AXIS#.IL.AINSOURCE
Description
This parameter sets which analog input to use for AXIS#.IL.AINSCALE.
| Value | Description |
|---|---|
| 0 | Uses no analog input. The current command in analog torque |
| 1 | Uses AIN1 |
| 2 | Uses AIN2 |
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 | |
| Added value '0' to range | 02-07-02-000 |
General Information
|
Type |
Read/Write |
|
Units |
N/A |
|
Range |
0 to 2 |
|
Default Value |
0 |
|
Data Type |
Integer |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.